DIO#.INV

Description

Sets or gets the polarity of a bi-directional IO when configured as a digital input (see DIO#.DIR).

Value Description
0 - Active high The digital input state is 1 when voltage is applied to the IO pin
1 - Active low The digital input state is 1 when voltage is removed from the IO pin

Examples

Usage

When DIO#.DIR = 0 (input) then the corresponding DIO#.INV can be set to change the polarity of the input signal.

Code

--> DIO1.DIR 0

With 24V on DIO1:

--> DIO1.INV 0 //Active high
--> DIO1.STATE
1
--> DIO1.INV 1 //Active low
--> DIO1.STATE
0

With 0V on DIO1:

--> DIO1.INV 0 //Active high
--> DIO1.STATE
0
--> DIO1.INV 1 //Active low
--> DIO1.STATE
1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosedPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen DIO1.INV 0x368A 0x2 USINT - - RW False
DIO2.INV 0x368B 0x2 USINT - - RW False
DIO3.INV 0x368C 0x2 USINT - - RW False
DIO4.INV 0x368D 0x2 USINT - - RW False
DIO5.INV 0x368E 0x2 USINT - - RW False
DIO6.INV 0x368F 0x2 USINT - - RW False